ContentPage

Alles over interne lagerspeling

Decoding rolling-element bearing numbers



With bearings being used across such a wide range of industries and applications, you would expect their design to be fully standardized and to have to comply to very strict international regulations. However, only a part of a bearing’s designation is currently regulated by standards issued by international bodies like ISO or ANSI.

This leaves manufacturers plenty of space for innovation and for coming up with designs that are specifically engineered to help distinguish themselves from other producers, while facilitating international bearing interchangeability and economical bearing production.

For consumers though, the lack of stricter standards means a multitude of unique part numbers that are specific to each manufacturer. These series are engraved or stamped on the products and can be easily retrieved when replacing a bearing. Still, if you plan to switch to a different brand or product, you need to know what the bearing designations mean in order to find suitable alternatives.

So how do you navigate the seemingly chaotic bearing designation systems?


What do numbers in bearing series codes mean?


In our Guide to bearings, we’ve detailed the various types of bearings used in industrial applications and their structural and functional differences. In this article we’ll focus only on rolling-element bearings (ball bearings and roller bearings). If you’re not yet familiar with this type of bearing, go ahead and read our beginner’s guide first.

Now let’s see how to read the roller bearing designations for some of the most popular brands on the market!

Typically, a roller bearing’s designation includes a basic number (designation), surrounded by supplementary codes - suffixes and prefixes. The suffixes and prefixes describe the tolerance, internal clearance and other design particularities.


The basic designation contains 3 to 5 digits and gives general information about the bearing, describing its:

  • type
  • boundary dimensions – width (B, C, T or H), outer diameter (D), bore diameter (d), chamfer dimension (r)
  • series number
  • contact angle

So a typical basic bearing designation looks like this: A BC DE, where:

  • A – Bearing type
  • B – Width
  • C – Outer diameter
  • DE – Bore diameter

Bearing series codes meaning

The boundary dimensions that are internationally standardized include the width and the outer diameter (B, C). Together, these are also referred to as the dimensional series of the bearing. The dimensional series (BC) along with the bearing type (A), so the first three digits of the number, form the bearing series symbol (A BC).

The bore diameter is given as a 2-digit code (DE), which needs to be multiplied by 5 to give the actual bore diameter in mm. However, this rule only applies to bore diameter dimensions greater than 20 mm. Under this value, the bore diameter uses the following code identifications:


Bore diameter 10 mm 12 mm 15 mm 17 mm
Code 00 01 02 03

When suffixes and prefixes are added, the bearing designation will look like this: Prefix A BC DE Suffix

The suffix can be separated from the rest of the designation number by a space, a hyphen or an oblique stroke. The codes for bearing types are as follows:


Bearing type SKF NSK Timken FAG
Double row angular contact ball bearing 0 3, 5 3
Self-aligning ball bearing 1 1 1, 2 1
Spherical roller bearing, spherical roller thrust bearing 2 2 2 2
Tapered roller bearing 3 3 3 3
Double row deep groove ball bearing 4 4 4
Thrust ball bearing 5 5 5 5
Single row deep groove ball bearing 6 6 6 6
Single row angular contact ball bearing 7 7 7 7
Cylindrical roller thrust bearing 8 8
CARB toroidal roller bearing C
Cylindrical roller bearing. Two or more letters are used to identify the number of the rows or the configuration of the flanges N NU, N, NU, NN NU, NN, N, NF N, HCN, NN, NNU
Four-point contact ball bearing QJ QJ
Tapered roller bearing in accordance with ISO 355 00 01 02 03
Separable ball bearing BO, E, L

As you can see, these codes are fairly agreed upon throughout the industry.


  • The letters BC in the code above indicate how wide the bearing is, and what the external diameter is.
  • For the outer diameter, the series numbers go from 7 – 8 – 9 – 0 – 1 – 2 – 3 – 4, with 7 being the smallest and 4 being the largest diameter.
  • For the width of radial bearings, the codes go from 8 – 0 – 1 – 2 – 3 – 4 – 5 – 6, with 8 being the smallest and 6 the biggest.
  • For the height of thrust bearings, the codes go from 7 – 9 – 1 – 2, with 7 being the smallest and 2 the biggest.

When it comes to suffixes and prefixes, things vary much more. Prefixes are used for defining the components of a bearing or variations. Suffixes are used to indicate design particularities such as the bearing internal design or external design (seals, snap ring groove), cage design, materials and heat treatment, the tolerance, clearance, preload and so on.

Below you can find common suffixes and prefixes used in roller bearing designations.


Prefixes - NSK Bearings

Meaning Bearing with special dimensions Bearing with flanged outer ring Higher load rating Miniature metric bearing with special dimensions Bearing outer ring with rollers and cage, no inner ring Miniature bearing made from extra corrosion-resistant steel
Code B F HR MR R -H-

Suffixes - Clearance

Meaning Normal radial internal clearance (RIC) Radial internal clearance smaller than C2 Radial internal clearance smaller than normalRadial internal clearance greater than normal Radial internal clearance greater than normal Radial internal clearance greater than C3 Radial internal clearance greater than C4
Code C0 / CN C1 C2 C3 C4 C5

To learn more about the bearing clearance and its values, read our article Bearing clearance: everything you need to know.


Other suffixes from various brands

Meaning SKF NSK Timken FAG
Angular-contact ball bearing with 30° contact angle A A T
Angular-contact ball bearing with contact angle of 25° ACD A5 A E
Angular-contact ball bearing with contact angle of 40° B B J B
Double-row angular contact ball bearing with contact angle of 25° B B B
Universal angular-contact ball bearing with contact angle of 40° BG, B(E)C BG, BWG BUA
Angular-contact ball bearing with contact angle of 15° CD C C
Spherical roller bearing with high load capacity, machined cage CA
Spherical roller bearing with high load capacity, pressed cage CD
Deep groove ball bearing with d <10mm and contact seal on one side RS1 D RSR
Deep groove ball bearing with d <10mm and contact seal on both sides 2RS1 DD 2RSR
Deep groove ball bearing with contact seal on one side RS1 DU RSR
Extra capacity design E E E
Tapered bore (taper 1:12) K K K
Solid brass cage, rib-guided MA (MB) M MA (MB)
Solid brass window-type cage MP MA1 MP
Solid brass cage, outer ring rib-guided MA6 MB M1A
Solid brass cage, guided by rolling elements M MR M
Bearing with snap ring groove in the outer ring of the bearing N N N
Polymer cage T T T
Pressed steel cage, one-piece J W J
Full complement roller bearing V V V
Non-contact seals on both sides 2RZ VV PP 2RSD
Deep groove ball bearing with single shield Z Z D Z
Deep groove ball bearing with double shield ZZ ZZ DD ZZ
External dimensions in line with ISO X X X



Do you have questions about our products?
For personal advise and product knowledge, visit an ERIKS location near you or contact our product specialists.

Find a service center | Call us | Send us an e-mail



LEARN MORE ABOUT BEARINGS

Bearings mounting guide: methods and tools

Improper handling or incorrect mounting and dismounting can damage the elements of a bearing, causing excessive noise and vibration levels. Learn how to properly mount bearings in this article.

Read now
Engineering Basics: Guide to Bearings

The purpose of this guide is to help you get familiar with the most common types of bearings, their design particularities and operating mode, the way they handle forces, the proper installation and maintenance procedures, as well as the most frequent problems that can cause the damage of bearings inside a machine.

Read now