CategoryPage
Hoses Selector
Are you looking for a particular type of hose? Find our full range of hoses here! Use the filters to search what you are looking for. Not sure what you need? Contact us , either through the chat or by phone and we will connect you with one of our specialists, they will be happy to advise you!
Medium
 
The Medium is the substance that will be transported through the hose. Some examples are : Oil , Castor Oil, Water , Chromid Acid or Citric Acid. Currently the list consists of over 400 mediums and we will be adding even more. Just start typing and the list will try to autocomplete the medium that you are looking for.
What is the medium would you like to transport?
Pressure
 
When transporting a medium, this is done under pressure. In this field, please provide the pressure (in bar) (assuming that the temperature of the medium is 20 degrees Celsius) which will be used to transport the medium. Examples are: 0,5 or 1,2
What is the minimal pressure (in bar) at which you want to transport the medium ?
bar
Temperature
 
Please provide the minimum and maximum temperature of the medium (in degrees Celsius ) that you will be transporting.An example can be : Minimum Temp: 0 and Max Temp : 65. Should you need to enter a negative value, please use a minus in that case, e.g. -10
What is the temperature range (degrees Celsius) at which you want to transport the medium?
°C
to
°C
Inside Diameter
 
Please provide the value of the inside diameter of the hose in mm. Examples are : 25, 50 , 125
What is the minimal inside diameter of the hose you are looking for?
mm

Industrial Hoses (23 products containing 172 Items)


Grid    
List    
1 / 3
Next
Grid    
List    
1 / 3